Recipe formulations

Recipe formulations

Recipe formulations build a common recipe that can make a variety of products by changing recipe input parameters. Users build and save a recipe formulation, and then select from the list of saved formulations when adding a batch to the batch list.
Consider the following when using recipe formulations:
  • Formulations only apply to recipes. They cannot be written for manually running operation sequences or phases.
  • Formulations only apply at the highest level of the control recipe. Recipes within a control recipe cannot use its formulations.
  • Formulations are optional. Master recipes without a formulation run with the formula values in the Master recipe.
  • Formulations not specified when creating a batch run with the default formula values from the Master recipe.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal