- FactoryTalk Batch
- Recipe Editor
- FactoryTalk Batch Equipment Editor
- Parameters and reports with FactoryTalk Batch
- Phase class overview
- Configure phases
- Operation sequence class configuration
- Operation sequence configuration
- FactoryTalk Batch View
- PhaseManager
- FactoryTalk Batch phases in Logix Designer
- Data from FactoryTalk Batch Server
- FactoryTalk Event Archiver
- FactoryTalk Batch administration
- FactoryTalk Batch security
- FactoryTalk Batch electronic signatures
- The FactoryTalk Batch Service Manager
- The FactoryTalk Batch Server
- FactoryTalk Batch Server option configuration
- PC-based phases introduction
Add the Batch Phase Execution control to a Microsoft Visual Basic project
The
Batch Phase Execution
control must be added to the Visual Basic
toolbox in order to make it available to your project. The instructions included here define the steps for manually adding the control to the toolbox after starting a new project. However, if you choose, you may configure the control to load automatically.To add the Batch Phase Execution control to a Visual Basic project
:- StartVisual Basic.
- From theProjectsmenu, selectComponents.
- On theComponentsdialog box, select theControlstab. The available Custom Controls are displayed in a list.
- Scrolling through the list, locate and select theBatch Phase Executioncontrol.
- ClickOKto close the dialog box. TheBatch Phase Executioncontrol is available on theVisual Basictoolbox. It is marked with a picture of a valve.
Provide Feedback