Configure Batch clients on Windows XP

Configure Batch clients on Windows XP

If a
FactoryTalk Batch
client is running on Windows XP Professional SP3 and connecting to a remote
FactoryTalk Batch
Server, you must change the
Local Security Policy
on the client computer. To allow the
FactoryTalk Batch
View to connect to a remote
FactoryTalk Batch
Server complete to the following steps.
  1. Point to
    Control Panel
    >
    Administrative Tools.
    Click
    Local Security Policy
    . The
    Local Security Settings
    window opens.
  2. Expand
    Local Policies
    , and then click
    Security Options.
  3. Locate and double-click
    Network access: Sharing and security model for local accounts
    . The
    Network access: Sharing and security model for local accounts
    dialog box opens.
  4. Select
    Classic - local users authenticate as themselves
    from the list.
  5. Click
    OK
    to close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal