webm file example

webm file example

The following example shows a movie clip (.webm) file added to an eProcedure manual instruction control step.
webm file example (1)
The HTML code that inserts the .webm file into the instruction file resembles the following:
<form> Prepare <sop>UNIT</sop> for delivery of <sop>ADD_AMOUNT.value</sop> KG of Egg. <br /><br /> Press OK to proceed. </form> <form> Begin charging <sop>ADD_AMOUNT.value</sop> KG of Egg into <sop>UNIT</sop> <br /><br /> Press OK when complete. <br /><br /> <video width="200" height="200" preload="auto" controls loop > <source src="customercontent\videos\clock.webm"> <source src="customercontent\videos\clock.ogg"> Video not supported in your browser </video> </form>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.