Configuring the material display

Configuring the material display

You can display the materials in list form (default) by type or by class. If you choose to display by type or class, you can select to display only certain types or classes of materials.
  1. From the
    User Preferences
    dialog box select the
    Materials
    tab.
  2. In the Materials Display Format area select the desired display format:
    • List
      (default)
      Displays the materials in alphabetical list form (as shown)
      FTB_filter_list
    • By Type
      Displays the materials by their type (for example; Finished, Intermediate, or Raw) or you can select all three to display the materials in a hierarchy view by type (as shown).
      FTBMM_list_filter_type
    • By Class
      Displays the materials by their class designation (for example; Colorings, Flavorings, etc.) or you can select all classes to display the materials in a hierarchy view by class (as shown).
      FTBMM_list_filter_class
  3. Click
    Apply
    . The Material list is refreshed, with the display format applied.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.