- Configuring materials
Run in simulation mode
Running a recipe in simulation mode is a good way to test the recipe. In this section, you use the .
sim
file for the ice_cream2.cfg
file, which is already configured to run the Chocolate Hazelnut recipe.- SelectStart > Rockwell Software > Simulator.
- SelectIMPORTANT:Administrator privileges are required to perform this procedure.File>Open. TheOpen Simulator Configuration Filedialog box opens.
- From theLook inlist, open thec:\Program Files\RockwellSoftware\ Batch\SampleDemo2\ Recipesfolder. Select theice_cream2.simfile, and then clickOpen.
- Minimize thePhase Simulatorwindow.
Provide Feedback