Add a server
Use the Network Editor to add a previously undefined server.
To add a server
:- Open theNetwork Editor.
- In theHierarchypane, select the type of server to add.
- ClickAdd Server.
- In theAliasbox, type an alias name. This is the name that displays in the Network Editor.
- In theComputer Namebox, type the computer name, or use the browse button to locate and select the computer from the list of computers on your domain.
- Click theSynchronizebutton.
- ClickOK.
Provide Feedback