Menu bar and toolbar
The menu bar contains the menus for
File
, Edit
, View
, and Help
.- File menuFrom theFilemenu, you can select a Network Model, synchronize all servers, print, and exit the Network Editor application.
- Edit menuFrom theEditmenu, you can add or remove a server from the Network Editor.
- View menuFrom theViewmenu, you can show or hide the toolbar/status bar, and refresh the Network Editor. You can also specify how data is viewed in the panes as well as setting other user preferences.
The Network Editor includes a toolbar which allows you to perform various functions. The buttons are enabled based on the item currently selected in the Network Editor. As you move your cursor over a button, a tool tip displays the button name and a detailed functional description displays in the status bar.
The Network Editor Toolbar buttons are:
![]() | Select Network Model : Allows you to select a network model from another computer. |
![]() | Synchronize : Allows you to synchronize your application servers. |
![]() | Add Server : Allows you to add a previously undefined server. |
![]() | Remove Server : Allows you to remove a server. |
![]() | Up One Level : Moves you up one level in the Hierarchy pane. |
![]() | Print : Prints a report for the selected item. |
![]() | Print Preview : Allows you to view a report on the selected item. |
![]() | Help : Opens the Network Editor help. |
Provide Feedback