Print reports

Print reports

The Network Editor report printing feature allows you to print network, server, or result pane information, in a report formatted with headers, footers and column headings (in list reports).
To print reports
  1. In the Network Editor’s Hierarchy pane, select the list or item(s) that you want to print.
  2. From the
    File
    menu, click
    Print
    . You could also click the
    Print
    button or press ctrl+p to display the
    Print
    dialog box.
  3. Ensure that the correct printer is selected, and click
    OK
    .
    TIP:
    To configure heading and footer fonts and add a custom footer to your reports, see Set report preferences
    Set report preferences
    for instructions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal