Edit the application font
The Network Editor defaults to the current Windows fonts. You can change the display font.
To edit the application font
:- Open theNetwork Editor.
- From theViewmenu, selectUser Preferences.
- On theGeneraltab in theUser Preferencesdialog box, selectUse application font.
- Select theFonttab.
- Select the desired font, style, and size from the appropriate lists, and then clickOK.
- ClickApply.
- ClickOK.
Provide Feedback