Start the Software

Start the Software

  1. Double click
    on the Data Explorer shortcut icon on your desktop to start Data Explorer (or under Start > Programs > Rockwell Software > Data Explorer 2.1.0.
    Data Explorer EXE
  2. Create a New Project by
    entering
    a name (e.g. TechEd) and
    selecting
    OK.
    New Project
  3. Data Explorer is open. We need to add data from various sources such as csv or EXCEL common extraction formats from different archives.
    Select
    the “Import to Dataset” (Wizard) icon and “Import to Dataset”. The data importer is very flexible (to support all format types, but some steps are involved).
    Import to Dataset
  4. Select
    Yes.
    Save Project
  5. Select
    Browse, “This PC”, “OSDisc (C:)” or other. And make a folder for training or tutorial and select “OK”.
    Browse Project Folder
    Locate Project Folder
  6. From the wizard we must first select the files to import.
    Select
    Add.
    Add Dataset
  7. Move
    to the C:\Program Files\Rockwell Software\FactoryTalk Analytics Data Explorer\2.1\samples folder and
    Select
    TurbineEmissionsAnalyzer.xls, and TurbinePlantData.csv and
    click
    Open. For simplicity in the lab (i.e. consistency with graphic images) select files in the order shown (TurbineEmissionsAnalyzer first).
    You may use Ctrl-Click for multi-select or Shift-Click for range select, open to complete your data file list.
    Import Datasets - Select Files
  8. Select
    the middle, second sheet on your XLS format file of emissions, “UnitNH3”. Then
    select
    “Remove”. We will in this tutorial skip the SCR data.
    Import Datasets - Add/Remove Files
  9. Select
    “Next”. Data import will be set up sequentially.
    Import to Dataset - Selected Files
  10. Select
    Next.
    Note that the wizard steps you through formatting steps to interpret your data properly (as intended). The first step is a raw file list/preview. There are cases where understanding how the raw data appears is useful in the ‘File Structure’ step. Note Turbine Emissions Analyzer data is captured every 30 seconds.
    Import to Dataset - Raw Data
  11. Select
    Next.
    The first step determines the column delimiter with an attempt at automatic detection (correctly here as a comma). Header rows are generally the label (Name) assumed first full header row. Properties (may be more than one that contain column information/not data) or Skip. Green are editable fields on the wizard.
  12. Select
    Next. Note your timezone may be different than shown.
    Import to Dataset: File Structure
  13. Confirm
    that the identified column formats (initial estimate) are correct. Note that the date/time format interpreted (column 1) is not correct.
    Select
    the Data Type under the first Column and
    change
    it from “String” to “DateTime”.
    Import to Dataset: Format Columns
  14. Select the Format Date option and update date time format to match to actual date time format. Modify Date Time Format as shown to match the uploaded data.
    Edit DateTime Format
  15. Scroll
    to the right to check further columns.
    Note the red highlighted tags indicated as ‘Unknown’ tags. Values that are blank for the initial (lengthy) period are Unknown (and red). As these tags are ppmvd and %vd (parts per million, volumetric dry and percent volumetric dry) units, we will assume these are not string tags, but Double (real) tags that are gathered (measured or archived) after the start of our data collection.
    Change
    each DataType to “Double” by
    selecting
    “Choose Data Types” button (default will be Float) or
    select
    the first leftmost red format,
    scroll
    to the far right format and
    select-the-range
    with a Shift-left-mouse click. Then
    press
    your spacebar and select “Double-Float”.
    Select
    Next. Once the active progress step no longer shows a problem (red-X).
    Import to Dataset: Add Data format for Unavailable Data
    Or (
    mouse click
    on leftmost Unknown,
    scroll
    right,
    Shift-mouse click
    , then spacebar &
    select
    Double-Float) and
    Select
    OK.
    Import to Dataset: Multi-select and Spacebar is a Hotkey for Multi-Change in Tables
  16. A caution icon in the far left column and yellow highlighted fields indicates there is an uncertainty and indicates this column may be (and is) our Time Column. You should select “Reassign Date and Time” to change or modify individual (Yellow) columns.
    Import to Dataset: Suggesting Time Column Assignment
  17. Where more than one Time column was available, you could select other than the first, leftmost Time Column (the default).
    Select
    Next.
    Import to Dataset: Assign Time Columns
  18. You may label ‘other’ Properties by
    selecting
    the label assigned “Property2” and changing it to your preference.
    Enter
    the text Units (or your preference).
    Select
    Next.
    Assigning a property name that is common across multiple data files allows you to use (e.g. on labels) or search for common data based on selected properties. This will be more and more useful as the available types of meta-data (data about your data) can be used to set up streaming applications.
    Import to Dataset: Label Data Property Information
  19. Review
    your format.
    Confirm Time and other cells appear correct. Note you may return to any step by selecting the wizard progress tree on the left if needed to correct a step. You may also return to this step once corrections are made. If all looks correct,
    select
    “Next” to proceed to the next data file and “Next”
    again
    to start with our second File Structure specification. Plant data is gathered every 5 seconds.
    NOTE:
    You may jump ahead or back at any time leveraging the import agenda on the left.
    Import to Dataset: Preview Import Results
  20. Change
    row 1 to ‘Column Name’.
    Select
    Next.
    The import selected row 2 to Name, because of problems we’ll correct next on row 1. Only one row can be a name, so once Row 1 is selected, Row 2 is changed automatically to a Property.
    Import to Dataset: Reassign Column Name
  21. Note
    that the DateTime format appears correct, but there is a problem indicated (red X) with potentially other problems indicated by the Red X.
    Scroll
    right with the bottom scroll bar until the first problem is indicated.
    Import to Dataset: Format Column Data
  22. The first problem we see is about halfway across. An unknown column type (labelled %), indicates “Data Type Must be selected”. Because we want to
    change
    this to Double-Float
    select
    “Choose Data Types” from the box in the upper right.
    Continue scrolling
    to the far right.
    Import to Dataset: Missing Data Type
  23. More Red columns after about two thirds of the columns and at the far right, indicate a problems with the column Names. You may
    put
    your cursor over the red cell and a pop-up detailed error message indicates that names 'cannot contain the character (")'. The string text within the csv ends with double “(one for end of string, one for inches H2O). The last column (if you
    put
    your cursor over the error indicator) indicates a duplicate name of a previous column.
    Select
    “Correct Column Names”, which fixes these issues (duplicate names with _2). Alternatively you may edit duplicate or non-allowed name strings where desired.
    Select
    Next twice (or simply select the next “Define Custom Properties”).
    Import to Dataset: Data Name Problems
  24. Change
    the Property Names to “Hist Tag” and “Units”. You may
    select
    “Start Import” or select Next. You may always jump to any previous step to repair data prior to import.
    Import to Dataset: Change Property Labels
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.