tmerge(valueVar-self,dtVar,method,interval,maxTimeGap,
handleDuplicates, handleOutOfOrder,maxCert)
This transform is
like $TimeMerge. It takes as input a variable that has numeric or
string values and a date/time variable, and merges the value variable
to match the date/time variable. Unlike the system-generated $TimeMerge,
it does not delete the value variable's original date/time column.
The additional arguments are the same as for $timemerge. The output
variable must be the same as the input value variable.
Provide Feedback