Add Application
You can register applications in FactoryTalk DataMosaix. DataMosaix allows you to register applications and generate credentials. The registered applications can be used to visualize data from FactoryTalk DataMosaix.
- On the Management Console, select theApplicationstab.The Applications list displays.Application Tab
- Click the [Add] icon.TheApplications Detailscreen displays.Application Detail screen
- Provide a unique and meaningful name for your Application. The Application Name works as the identifier for your application. You can search for an application with the App Name. By default, FactoryTalk DataMosaix populates an application name.Application Name example: APP_1206230756_createproject_v1.Here, APP stands for application, 120623 is the date in ddmmyy format, 0756 is the timestamp in hhmm format, and createproject_v1 is the project in which you are currently working. You can use the default App Name or create your own.
- Provide the URL of the application.
- Provide a description for the application.Add Application Details
- Click [Save and Create Credentials] to register the application.TheCredentials and other infodialog box displays the client secret information.Client Secret InformationNOTE: It is important to copy and save the credentials in a file immediately for future use. Once you close theCredentials and other infodialog box, this information cannot be viewed later. If you fail to save the client secret information, you will have to regenerate the secret.Copy the credentials and insert them in the application for it to connect to FactoryTalk DataMosaix.
- Click [Copy All].
- Open a text file, paste the client secret, and save the file.
- Click [Close and Go to Listing].The new application displays under Application Listing.Application List
Provide Feedback