Edit Application
- On the Management Console, select theApplicationstab.The Applications list displays.Application List
- In theActionscolumn, click the [Edit] icon next to the application that you want to edit.Edit iconThe Application detail screen displays.You can edit the application information such as Application Name, Application URL, and Description.Edit Application screen
- Edit the information in the required fields.
- Click [Save Changes].TheApplicationstab displays the updated information for the edited application.Edited Application
Provide Feedback