Edit Extractor
- On the Management Console, select theExtractor Infotab.The Extractors list displays.Extractor Listing
- In theActionscolumn, click the [Edit] icon next to the extractor that you want to edit.TheExtractor Detailscreen displays.Extractor Detail screenYou can edit the extractor information such as source name, Location, Pipeline, and Source Type.
- Edit the information in the required fields.
- Click [Save Updates].
Provide Feedback