Regenerate Secret for Extractor
- On the Management Console, select theExtractor Infotab.The Extractors list displays.Extractors List
- In theActionscolumn, click the [Edit] icon next to the extractor for which you want to regenerate the client secret.TheExtractor Detailscreen displays with the existing client secret and the [Regenerate Secret] link.Extractor Details
- Click the [Regenerate Secret] link.A confirmation box displaysRegenerate Secret Confirmation box.Generating a new client secret makes the existing client secret invalid. After generating the new secret, you must update the information in the required files.
- Click [Yes, Regenerate].Regenerate Extractor Client Secret
- Click the [Copy] icon to copy and save the new client secret.NOTE: It is important to copy the client secret and update it in the related files. Once you close this screen, this information cannot be viewed later. If you fail to save the client secret information, you will have to regenerate the secret.
- Open a text file, paste the new client secret, and save the file.
- Click [Done].
Provide Feedback