Launch FactoryTalk DataMosaix from FactoryTalk Hub
- Navigate to FactoryTalk Hub sign-in screen.FactoryTalk Hub sign-in screen
- Click [SIGN IN].The Sign in page displays.Rockwell Automation sign-in screen
- Provide your MyRockwell credentials.NOTE: Click [Create an Account] if you are a new user.
- Click [Sign in].The FactoryTalk Hub dashboard displays. It shows all the applications offered based on your subscriptions and entitlement.FactoryTalk Hub Home Screen
- Click theOperationstab.You should be able to see all the applications in the Operations category.NOTE:
- If you see the FactoryTalk DataMosaix tile is locked, it means your organization has not purchased the entitlement for this application.
- If you are sure that your organization has purchased the entitlement, but you do not see the FactoryTalk DataMosaix tile, then you must ask the administrator to add you to the FactoryTalk Hub organization.
FactoryTalk Hub Operations Tab - Click theFactoryTalk DataMosaixtile.The FactoryTalk DataMosaix application opens in a new tab. TheApplicationstab displays by default.FactoryTalk DataMosaix Home Screen
Provide Feedback