Assign Role
FactoryTalk Data Mosaix provides a set of predefined roles that enable members to perform tasks based on their assigned roles. For example, a member who is a project administrator can modify roles for other members. A project admin can allow members to perform certain functions or limit members from doing classified actions.
- On the Management Console, select theManage Accesstab.Member Listing
- In theActionscolumn, click the [Add] icon next to the member for whom you want to assign roles.If all the roles are already assigned to the member, the [Add] icon is disabled. If there are some roles unassigned to the member, the [Add] icon is enabled.TheAdd Rolesscreen displays. This screen displays a list of roles that you can assign.Add RolesNOTE: The existing roles assigned are not displayed here. You can view the existing roles in theRolescolumn under Member Listing.
- Select the checkbox adjacent to the role name to assign the role.You can select multiple roles by selecting the required checkboxes. To assign all the available roles, select the [Select all] checkbox.
- Click [Add].The Member Listing displays. Under Member Listing, you can view the assigned roles in theRolescolumn.Assigned Roles
Provide Feedback