Edit Role
If you are a project administrator, you can modify the assignment of roles. You can either assign a role or remove an existing role for a member.
- On the Management Console, select theManage Accesstab.Member Listing
- In theActionscolumn, click the [Edit] icon next to the member.NOTE:
- If no roles are assigned, the [Add] icon is enabled
- If all roles are assigned, the [Add] icon is disabled.
- If there are some roles unassigned, then both, [Add] and [Remove] icons are enabled.
TheEdit all Rolesscreen displays. This screen displays the assigned and unassigned roles.Edit Roles - Select the checkbox adjacent to a role to assign it.
- Clear the selection from a checkbox to remove the role.
- After you make all the changes, Click [Apply].The Member Listing displays.
- View the modified roles in theRolescolumn.
Provide Feedback