Remove Role
If you are a project administrator, you can remove any or all of the assigned roles.
- On the Management Console, select theManage Accesstab.Member Listing
- In theActionscolumn, Click the [Remove] icon in front of the member.NOTE: If any or all roles are assigned to the member, the [Remove] icon is enabled. If no roles are assigned to the member, the [Remove] icon is disabled.TheRemove Rolesscreen displays. This screen displays the assigned roles.Remove Roles
- Select checkbox adjacent to a role.You can select multiple roles by selecting the required checkboxes. To remove all the assigned roles, select the [Select all] checkbox.
- Click [Remove].The Member Listing displays. Under Member Listing, you can view that the removed roles are not shown in theRolescolumn.
Provide Feedback