Remove Roles from Multiple Members
If you are a project administrator, you can remove assigned roles from multiple members using this feature.
- On the Management Console, select theManage Accesstab.
- To remove roles from multiple members, select the checkboxes adjacent to the members' names.Bulk Remove Roles from MembersThe [Add] and [Remove] icons above the member grid are enabled or disabled, based on the roles assigned to the selected members.
- If no roles are assigned to any the selected members, the [Add] icon is enabled and [Remove] icon is disabled.
- If all the roles are assigned to all the selected members, the [Add] icon is disabled and [Remove] icon is enabled.
- If some roles are assigned to any of the selected members, then both, [Add] and [Remove] icons are enabled.
- Click the [Remove] icon above theMember Namecolumn.TheRemove Rolesscreen displays the list of available roles with a number next to each role name. The number in the parentheses (), denotes how many members out of the selected members are currently assigned a role.Bulk Remove Roles
- Select the checkboxes adjacent to the roles you want to remove. Selecting the checkboxes will remove those roles from the members that are currently assigned the roleYou can assign all the available roles, by selecting the [Select all] checkbox.
- Click [Remove].The Member Listing displays. Under Member Listing, you can view that the removed roles do not appear in theRolescolumn for the selected members.Multiple Members - Removed Roles
NOTE:
Click here for information on CDF Access Management.
Provide Feedback