Edit Asset
You can edit an existing asset by updating the properties of the asset.
- On the Management console, select theModelingtab.The Model Listing page displays the available assets.Model Listing
- Select an asset node.
- Click the Edit icon.TheModel Item Detailpage displays.Model Item Detail screen
- Modify the required asset information and clickSave.The updated asset is displayed in the asset list.NOTE:
- You can move an asset from one parent node to another parent node by using the drag-drop action.
- Moving an asset node from one root to another root is not allowed.
- A parent node cannot be moved to a child node.
Provide Feedback