Delete Extractor
- On the Management Console, select theExtractor Infotab.The Extractors list displays.
- In theActionscolumn, click the Delete icon next to the extractor that you want to delete.TheExtractor Detailscreen displays.NOTE: Once you delete an extractor, the extractor can no longer be used for sending data to FactoryTalk DataMosaix. Deleting an extractor removes all the information including the client secret. Hence, before deleting an extractor, verify the information so that you delete the correct extractor.
- ClickDelete Extractorto proceed deleting the extractor.TheConfirm Deletiondialog box displays.
- ClickYesto delete the extractor.The extractor is removed from the Extractor List .
Provide Feedback