Register a Custom Extractor
This topic describes the steps to register a custom extractor in FactoryTalk DataMosaix. You can create a custom extractor if your source type cannot be used with any of the available extractors.
Prerequisites
- A project is created using FactoryTalk DataMosaix.
Register a custom Extractor
- On the Management Console, select theExtractor Infotab.The Extractor list displays.
- Click the Add [+] icon.TheExtractor Info Detailscreen displays.
- Provide a unique and meaningful name for your Extractor. The Source Name works as the identifier for your extractor. You can search for an extractor with the Source Name. By default, DataMosaix populates a source name.Source Name example: EXT_1406230728_createproject_v1.Here, EXT stands for extractor, 140623 is the date in ddmmyy format, 0728 is the timestamp in hhmm format, and createproject_v1 is the project in which you are currently working. You can use the default source name or create your own.
- Provide the location details for which you are creating the extractor. This is additional optional information that can help you identify an extractor when you have many extractors for different plants/sites/locations.
- From the Associated Roles drop-down list, select at least one role. You can refer to various roles and capabilities by clicking Role Reference.You can select multiple roles from the Associated Roles drop-down list. In the search bar, you can search for any specific role from the list. If you want to apply all the roles to the application, select theSelect Allcheck box.NOTE:The Associated Roles drop-down is visible and available only for Project Admin users or users within the Organization with a Project Admin Role assigned.Next, you can select a pipeline or create a new pipeline. When you create a new pipeline, you have the option of selecting from an existing dataset or creating a new dataset.
- From the pipeline drop-down, select a pipeline. On selecting a pipeline, the Pipeline External ID and Dataset Name fields are populated.To create a new pipeline, select the+ Create Pipelineoption.The Create Pipeline dialog box displays.
- Provide the following Pipeline information to create a new pipeline.
- Pipeline Name
- Pipeline External ID
- Pipeline Description
- When you create a pipeline, you can either select an existing dataset or create a new dataset. Select a Dataset from the drop-down if you want to use an existing Dataset.If you choose to create a new Dataset, the Dataset related fields are displayed. Provide the following dataset information.
- Dataset Name
- Dataset Description
- ClickAdd. Based on the options you choose (select or create), the Pipeline and Dataset information is either populated or created and displayed on the Extractor Info Detail page.
- Select the source type of extractor as Add Custom / Other.NOTE:TheSave and Applybutton enables after you provide all the required details.
- Provide the custom extractor name.
- Click Save and Apply.
- TheCredentials and other infodialog box displays extractor registration details.NOTE: It is important to copy and save the credentials in a file immediately for future use. Once you close theCredentials and other infodialog box, this information cannot be viewed later. If you fail to save the information, you will have to regenerate the client secret.
- ClickCloseto close the pop-up window.The new extractor is displayed under Extractor Listing.
Provide Feedback