Install FTOptix - DataMosaix Connector

Install FTOptix - DataMosaix Connector

On the Extractor Info Detail page, once you select the source type as FT Optix in the Source Info field, a link to download the Optix connector (Get FactoryTalk Optix DataMosaix Connector) is displayed, which you can use to download the Optix-DataMosaix connector installer file.
Perform the following steps to install FT Optix - DataMosaix connector:
  1. Download the Optix DataMosaix connector installer file (FTDataMosaix_Optix_Connector.msi) from the Product Compatibility and Download Center (PCDC). Also, you can use this link to download the connector.
  2. Right-click on the FTDataMosaix_Optix_Connector.msi file and choose
    Run as Administrator
    to begin the installation.
    The
    SOFTWARE AND CLOUD SERVICES AGREEMENT
    dialog box is displayed.
  3. Read the license agreement and select the
    I accept the terms in the License Agreement
    checkbox and then click
    Install
    .
    Installer Setup
    By default, the installation takes place in the following location:
    C:\Program Files\Rockwell Automation\FTDataMosaix_Optix_Connector
    .
  4. Once the installation is complete, the ‘Completed the FTOptix_DataMosaix_Connector Setup Wizard’ screen is displayed. Click
    Finish
    to close the installation window.
    After the installation is completed successfully, a shortcut to the ‘FactoryTalk Optix - DataMosaix Connector Setup’ will be created on your machine.
    Connector Setup Shortcut
  5. Double-click on the
    FactoryTalk Optix - DataMosaix Connector Setup
    to open it.
    The 'FactoryTalk Optix - DataMosaix Connector Setup' window is displayed.
    Optix - DataMosaix Connector Setup
    NOTE:
    If you see a message about needing .NET to run the setup, download and install the latest version.
  6. Specify the exact location of the Optix project by clicking
    Browse
    and provide the project folder path.
  7. Click
    Deploy Connector
    .
    Upon successful completion, you will see a dialog box stating
    'Configuration Completed. Click on Browse Another if you want to configure the connector for another project'.
  8. (Optional) Click
    Browse Another
    to configure the connector for another Optix project.
NOTE:
After setting up the FT Optix - DataMosaix connector, you must restart the FT Optix application for changes to take effect.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal