Set Client Credentials for Transformation

Set Client Credentials for Transformation

Perform the following steps to set client credentials for transformation:
  1. In the Mapping editor, click
    Run
    and select
    Run with client credentials
    .
    If the client credentials are not set, you can see the missing credentials dialog box. You need to set your client credentials before you can run a transformation.
    Mapping Editor
  2. Click
    Set client credentials
    .
    Missing Credentials Dialog
  3. On the
    Client Credentials
    dialog box, provide the client credentials that you saved when you registered an extractor earlier.
    Set Client Credentials
    Now you are ready to run the transformation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.