Select a data type

Select a data type for a tag or when creating or editing a member of a user-defined data type. Data types specify the size and layout of memory allocated for the tag. For more information, see Data types.
  1. In
    Select Data Type
    , select a data type from the list.
  2. (optional) In
    Search
    , begin typing the name of the data type to return data types that match the search criteria.
  3. (optional) If the usage of the tag is LOCAL or INOUT, under
    Array Dimensions
    , enter the array dimensions.
  4. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.