File Standard Deviation (STD)

File Standard Deviation (STD)

The STD instruction calculates the standard deviation of a set of values in one dimension of the Array and stores the result in the Destination.
The standard deviation is calculated according to this formula:
STD_Formula 1_v31
Where:
start = dimension-to-vary subscript of the array operand
xi = variable element in the array
N = number of specified elements in the array
AVE = STD_Formula 2_v31
IMPORTANT: Make sure the Length does not cause the instruction to exceed the specified Dimension to vary. If this happens, the Destination will be incorrect.
If an overflow occurs during expression evaluation or if the instructions reads past the end of an array, the instruction sets the ER bit and stops execution.
Available Languages
Ladder Diagram
Ladder_File Standard Deviation (STD)_v1
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversion.
Ladder Diagram
Operand
Type
Format
Description
Array
SINT
INT
DINT
REAL
array tag
Find the standard deviation of the values in this array
Specify the first element of the group of elements to use in calculating the standard deviation
Dimension to vary
DINT
immediate
(0, 1, 2)
Which dimension to use
The order of the dimensions is: array[0,1,2]
Destination
REAL
tag
Result of the operation
Control
CONTROL
tag
Control structure for the operation
Length
DINT
immediate
Number of elements of the array to use in calculating the standard deviation
Position
DINT
immediate
Offset into the specified array which identifies the current element that the instruction is accessing.
Initial value is typically 0
CONTROL Structure
Mnemonic
Data Type
Description
.EN
BOOL
The enable bit indicates the STD instruction is enabled.
.DN
BOOL
The done bit is set when the instruction has operated on the last element in the Array.
.ER
BOOL
The error bit is set when the instruction generates an overflow. The instruction stops executing until the program clears the .ER bit. The .POS value stores the position of the element that caused the overflow.
.LEN
DINT
The length word specifies the number of elements in the array on which the instruction operates.
.POS
DINT
The position word is an offset into the specified array which identifies the current element that the instruction is accessing.
Affects Math Status Flags
Major/Minor Faults
A major fault will occur if:
Fault type
Fault code
.POS < 0 or .LEN < 0
4
21
Dimension to vary > number of dimensions
4
20
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition / State
Action Taken
Prescan
The .EN bit is cleared.
The .DN bit is cleared.
The .ER bit is cleared.
Rung-condition-in is false
The .EN bit is cleared.
The .ER bit is cleared.
The .DN bit is cleared.
The .POS value is cleared.
The rung-condition-out is false.
Rung-condition-in is true
Internally, the instruction uses a FAL instruction to calculate the average:
Expression = standard deviation calculation
Mode = ALL
Postscan
N/A.
Examples
Example 1
Calculate the standard deviation of arrayDint, which is DINT[4,5].
STD_Example 1 dimension_v31
STD_Example 1 eqation_v31
Ladder Diagram
FTStudio STD EX1 V1
Example 2
Calculate the standard deviation of dint_array, which is DINT[4,5].
L5K_STD_Example 2 dimension_v31
Ladder Diagram
FTStudio STD EX2 V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal