Add Resource Meter

Add Resource Meter

Perform the following steps to add the Resource Meter to the hierarchy list:
NOTE:
The following point is required to view data on
Resource meter dashboard
:
  • Default unit should be configured for demand and consumption measurement with correct tag mapping.
  1. Select the
    Site
    or
    Area
    or
    Work center
    , or
    Work units
    and the [] icon appears.
  2. Click the [] icon and select [Add].
  3. In the
    Add Component
    dialog, select [Resource] under
    Meter
    from the left pane and set these parameters:
    • Resource Type
      : Select the type of resource from the drop-down list.
      Resource Meter types
    • Name
      : Provide the Resource meter name.
    • Description
      : Provide the description of the Resource meter.
  4. Click [Add].
    Add Resource Meter dialog
The "
Resource meter added under Site or Area or Work center or Work units successfully
" message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.