Move Component

Move Component

Perform the following steps to move the component in the hierarchy list:
  1. Select the required component and the [] icon appears.
  2. Click the [] icon and select [Move].
  3. In the
    Select Destination
    dialog, select the destination hierarchy level to move and click [Move].
    Select destination dialog
    The "
    Component moved under component successfully
    " message displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.