Time Picker

Time Picker

This feature allows users to adjust the chart time period across various dashboard levels (Enterprise, Region, Site, Area, Work Center/Work Unit).
Perform the following steps to change the chart time period in all the dashboard levels, such as
Enterprise
,
Region
,
Site
,
Area
, and
Work Center/ Work Unit
:
  1. Click the date and the
    Select Time Scope
    dialog box is displayed.
  2. Select the time period from the left panel of the dialog box. And select
    Date
    ,
    Week
    ,
    Month
    , and
    Year
    from the date picker.
  3. You can manually provide the
    From
    and
    To
    date and select the time stamp using the slider below.
    Select Time Scope
  4. Click
    Submit
    .
  5. User can also click the [] and [] icons to go to earlier or later dates, respectively.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal