Provide feedback

Provide feedback

Operations Hub includes an option for the User to provide feedback about their experience with the service to the FactoryTalk Hub team. Follow these steps to provide feedback:
  1. Navigate to the top banner and click the question mark (
    ?
    ) icon. A list of help options displays.
  2. Click
    Provide Feedback.
    The
    Feedback
    dialog box displays.
  3. Select a feedback topic from the pull-down list. The available options are:
    • Provide Feedback
    • Enhancement Request
    • Report an Issue
  4. Enter the details of your feedback, request, or issue into the space provided. A maximum of 1000 characters is permitted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.