- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Create a key value converter
Create a converter that changes Boolean values into localized text.
- InProject view, right-clickConvertersand select .
- Double-click the converter.
- In the central pane, set the following values:KeysBooleanValuesStringTrueTrueFalseFalseFor more information about dynamic links, see Create dynamic links.
Provide Feedback