Create a DataStore with sample data types
Create a database with sample data types to populate and export to a
CSV
file.- Create an Embedded database. See Create a database.
- Hover-over the database, select, and enterEditStore1.
- Configure the following table columns:Column numberData type1Int162Int323Float4StringFor more information, see Prepare a database table structure for population.
Provide Feedback