Configure the AlarmImporter NetLogic
Integrate the NetLogic with your project.
- InProject view, selectAlarmImporter.
- InProperties, at the top, select .
- Hover-over the variable, select, and enterEditCSVPath.
- SelectInt32and selectAbsoluteResourceUri.TIP: If you do not see the required option, select theShow allcheck box.
- Remove the variable value.The variable value is empty.
Provide Feedback