Configure the report footer
Configure the bottom part of the report.
- Create a divider:
- InProject view, right-clickFooterand select .
- SetBorder colorto#000000.
- SetFill colorto#000000.
- SetHorizontal alignmenttoStretch.
- SetHeightto0.019685mm.
- SetTop marginto0.375mm.
- Add page numeration:
- Right-clickFooterand select
- Hover-over the label, select, and enterEditPageNumeration.
- InProperties, create a dynamic link betweenTextand .
- SetHorizontal alignmenttoLeft.
- SetWidthto0.787402.
- SetTop marginandLeft marginto0.15.
- Add date stamp:
- Right-clickFooterand select
- Hover-over the label, select, and enterEditDateStamp.
- InProperties, create a dynamic link betweenTextand .
- SetHorizontal alignmenttoRight.
- SetWidthto1.5.
- SetTop marginandRight marginto0.15.
Provide Feedback