- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
RemoteVariableSynchronizer() constructor
Create a
RemoteVariableSynchronizer
object that can contain a list of project variables to be kept synchronized with the related field variables.public RemoteVariableSynchronizer()
Example
In the following example, a
variableSynchronizer
object is created to keep the value of a Speed
project variable synchronized with the value of a field variable that identifies the speed of a motor. The project variable, represented by the motorSpeed
object, is added to the variableSynchronizer
object via the Add()
method.When the field variable changes its value, the
motorSpeed_VariableChange
method is executed. When the value of motorSpeed
(of the field variable), is greater than 200, a warning message is generated.In the
Stop()
method, the termination of the synchronization when the NetLogic parent node is removed is effected by invoking the Dispose()
method.
IMPORTANT:
the
RemoteVariableSynchronizer
object must be declared as a class member within the NetLogic.private void Start() { motorSpeed = LogicObject.Owner.GetVariable("Speed"); variableSynchronizer = new RemoteVariableSynchronizer(); variableSynchronizer.Add(motorSpeed); motorSpeed.VariableChange += MotorSpeed_VariableChange; } private void MotorSpeed_VariableChange(object sender, VariableChangeEventArgs e) { if (motorSpeed.Value > 200) { Log.Warning("Speed limit reached!"); } } private IUAVariable motorSpeed; private RemoteVariableSynchronizer variableSynchronizer;
Provide Feedback