- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
ResourceURI.FromApplicationRelativePath(path)
Returns a C # object of the
ResourceURI
type, with the URIType
of ApplicationRelative
that contains a relative path to a file in relation to the ApplicationFiles
folder.static ResourceUri FromApplicationRelativePath(stringpath);
Arguments
- path(string)
- A relative path to a file in relation to theApplicationFilesfolder.
Returns
- ResourceURI
- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C#
applicationRelativeResourceURI
object of the ResourceURI
type that contains the Text1.txt
relative path. The object is used as an argument of the .NET WriteAllText API
to create a Text1.txt
text file inside theApplicationFiles
folder.
var applicationRelativeResourceUri = ResourceUri.FromApplicationRelativePath("Text1.txt"); Log.Info(applicationRelativeResourceUri.ApplicationRelativePath); File.WriteAllText(applicationRelativeResourceUri.Uri, "Hello world!");
Provide Feedback