- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
ResourceURI.FromURI(uri)
Returns a C# object of the
ResourceURI
type, with the URIType
type pf URI
and that contains an absolute path to a generic resource.Arguments
- uri(string)
- An absolute path of a generic resource, usually a network path or a website address.
Returns
- ResourceURI
- A C# object that contains the path indicated in the argument.
Example
Below is an example in which the API returns a C # website object of the
ResourceURI
type that contains the https://www.rockwellautomation.com/
URL.
var website = ResourceURI.FromURI("https://www.rockwellautomation.com/");
Provide Feedback