- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Access project nodes
You can access C# object members, OPC UA nodes, NetLogic objects, and session aliases.
C# object members
In C#, each property or method contained in an object is generically defined as a member of the object. Each member is identified by
BrowseName
of the matching project node.
TIP:
To display the
BrowseName
of a property, hover over its name in the Property
pane. A tooltip appears with the BrowseName
, data type, and short description (if present).To access the members in hierarchical order, use the point.
In the following example, The
Acceleration
property of the Motor
object is set to the value of 123
.
Motor.Acceleration = 123;
In the following example, the value of the
Motor
object Speed
property is assigned to the value of the currentSpeed
C# integer variable.
int currentSpeed = Motor.Speed;
OPC UA nodes of a FactoryTalk Optix Studio project
FactoryTalk Optix Studio
project To access a node in the C# information model, the node must be represented in the NetLogic by a matching C# object. To obtain the matching C# object, you can use these APIs:
To refer to the OPC UA nodes of the properties of a typed node, the name of the matching C# property consists of the
BrowseName
of the property to which the suffix is added. The following example shows a dynamic link set on theVariable
Text
property of a label through API, accessing the property node represented by TextVariable
.
Label1.TextVariable.SetDynamicLink(speedValue);
Provide Feedback