- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Asynchronous task
Create an asynchronous tasks to run code asynchronously.
TIP:
FactoryTalk Optix Studio
provides C# class specifications that exhibit the constructors that you can use for creating asynchronous tasks. The constructors are based on the .NET framework C# System.Threading.Tasks.Task
class, which represents an asynchronous task. See Task Class.Available classes
You can use these classes to create asynchronous tasks:
- PeriodicTask
- A task that runs code at regular time intervals.
- DelayedTask
- A task that runs code after a time delay.
- LongRunningTask
- A task that requires significant time or CPU resources.
Provide Feedback