- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Subscribe methods to events
When an object generates an event, the event data is displayed using a corresponding delegate event handler method.
You can subscribe methods to the following events:
- Change value of a variable.
- All events generated by an object.
- An event generated by an object.
Provide Feedback