- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Install NuGet packages in Visual Studio
Install NuGet packages by using NuGet Packages Manager.
Set Visual Studio as the default external code editor. See Set the default code editor.
- From the main toolbar, select
.
The default external code editor opens.TIP: We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. - Install the necessary NuGet packages. See Install and use a NuGet package in Visual Studio | Microsoft Docs
- Select the project to open theCSPROJfile.
- In theCSPROJfile, after the<AppendTargetFrameworkToOutputPath>false</AppendTargetFrameworkToOutputPath>property, add the<CopyLocalLockFileAssemblies>true</CopyLocalLockFileAssemblies>property.
- Save theCSPROJfile.
- Compile the project.
Provide Feedback