- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Configure the debugger
Configure the Visual Studio or Visual Studio Code debugger.
- From the main toolbar, select
.
The default external code editor opens.TIP: We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. - If you use Visual Studio:
- From theDebugmenu, selectAttach to Process.A window that shows all processes running on the machine appears.
- Next toAttach to, clickSelectand selectAutomatic. SelectOK.
- InAvailable Process, select either:
- FTOptixRuntime.exe
- Debugs a runtime NetLogic.
- FTOptixStudio.exe
- Debugs a design-time NetLogic.
- SelectAttach.The debug mode starts.
- If you use Visual Studio Code:
- Open theRun and Debugpane by pressing .
- From the list at the top of the pane, select either:
- Attach to FTOptixRuntime (NetSolution)
- Debugs a runtime NetLogic.
- Attach to FTOptixStudio (NetSolution)
- Debugs a design-time NetLogic.
- SelectStart Debuggingor press.F5
Provide Feedback