Edit the code after debugging

Edit the code after debugging

The initialization of the debugging process is different for design-time and runtime NetLogics.
  1. Select an option:
    • If you are debugging a NetLogic at runtime, from
      FactoryTalk Optix Studio
      toolbar, select the Stop icon.
    • If you are debugging a NetLogic at design time, in Visual Studio or Visual Studio Code, select
      to stop debugging.
  2. Edit the code and save the edited
    CS
    files.
    FactoryTalk Optix Studio
    automatically recompiles the .NET solution.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.