- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Add a third-party library to the Visual Studio Code project
Add a third-party .NET library by editing the
CSPROJ
project file.Set Visual Studio Code as the default external code editor. See Set the default code editor.
- Copy the .NET assembly for the library to theProjectFiles/NetSolutionFactoryTalk Optix Studioproject folder.
- From the main toolbar, select
.
The default external code editor opens.TIP: We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. - In Visual Studio Code, open theCSPROJproject file.
- Add the following<Reference>element as a child of the<ItemGroup>element.<Reference Include="library"> <HintPath>path</HintPath> <Private>False</Private> </Reference>
- library
- The library that you want to add. For example:MyLibrary
- path
- The path to the library from 1. For example:..\MyLibrary.dll
<ItemGroup> <Reference Include="MyLibrary"> <HintPath>..\MyLibrary.dll</HintPath> <Private>False</Private> </Reference> <!-- The rest of the code --> </ItemGroup> - Save theCSPROJfile.
Provide Feedback