Event logger
Records the properties of one or more event types of interest generated by a specific node and/or by its child nodes, or by any node in the project, and stores them in a database.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Locales | Locales | Locales of interest for storing translations of LocalizedText data in the database, typically the descriptions of the events. Each locale has an additional column in the database for each localized property. If empty, the locales are those expected by the project (Locales property of the project root node). | |
Event configurations | EventConfigurations | Event configuration collection of objects. If empty, record events generated by any project node. | |
Event arguments | EventArguments | ||
Event fields to log | EventFieldsToLog | Properties to record of the different events of interest. |
Provide Feedback