- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Multistate image
Based on the current state value, displays a specific image.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
State value | StateValue | Value of the current state. | |
States | States | List of states, each of which is associated with a specific image. | |
Path | Path | (Inherited from Image) | |
Dynamic color | DynamicColor | (Inherited from Image) | |
Fill Mode | FillMode | (Inherited from Image) | |
Hit test visible | HitTestVisible | (Inherited from Image) | |
Image left margin | ImageLeftMargin | (Inherited from Image) | |
Image top margin | ImageTopMargin | (Inherited from Image) | |
Image right margin | ImageRightMargin | (Inherited from Image) | |
Image bottom margin | ImageBottomMargin | (Inherited from Image) | |
Blink | Blink | (Inherited from Image) | |
Colorization mode | ColorizationMode | (Inherited from Image) | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Provide Feedback