- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Configure a Dropdown button
Configure a
Dropdown button
object by linking it with a container object type.- InProject view, create a container object type.For example, create aPanel (type)
- Create aDropdown Button.
- InProperties, create a dynamic link between thePanelproperty and the container object type.For more information about dynamic links, see Create dynamic links.
Provide Feedback