Enable accelerated software rendering
If you run
FactoryTalk Optix Studio
or FactoryTalk Optix Applications
inside a VMware®
hypervisor, you can enable accelerated software rendering of graphics and video.
IMPORTANT:
Enabling accelerated software rendering may negatively impact compatibility.
- On the system that runs hypervisor, in theVMwareVirtual Machine Settings, on theHardwaretab, selectAccelerate 3D graphics.
- On the virtualized Windows system, selectStart, search for and openView advanced system settings.
- InSystem Properties, on theAdvancedtab, selectEnvironment Variables.
- InEnvironment Variables, underSystem variables, setQT_OPENGLtoangle.
- InEnvironment Variables, selectOK.
- InSystem Properties, underPerformance, selectSettings.
- InPerformance Options, selectCustomand clearShow shadows under windows.
- InPerformance Options, selectOK.
- InSystem Properties, selectOK.
Provide Feedback